Radio Band Link

This is a source sequence parameter which is used by the test set's source to determine the channel plan to be used when computing the Frequency/Channel values.

Double-clicking in the Radio Band Link field opens a dropdown list of the choices: UP (equivalent to Mobile Station) or DOWN (equivalent to Base Transceiver Station). DOWN is the default value.